// this file is an archive of JavaScripts used for the EmersonProcessManagement suit of files 

function MM_swapImgRestore() { //Dreamweaver v3.0
  var i,x,a=document.MM_sr; for(i=0;a&&i<a.length&&(x=a[i])&&x.oSrc;i++) x.src=x.oSrc;
}

function MM_preloadImages() { //Dreamweaver v3.0
  var d=document; if(d.images){ if(!d.MM_p) d.MM_p=new Array();
    var i,j=d.MM_p.length,a=MM_preloadImages.arguments; for(i=0; i<a.length; i++)
    if (a[i].indexOf("#")!=0){ d.MM_p[j]=new Image; d.MM_p[j++].src=a[i];}}
}

function MM_findObj(n, d) { //Dreamweaver v3.0
  var p,i,x;  if(!d) d=document; if((p=n.indexOf("?"))>0&&parent.frames.length) {
    d=parent.frames[n.substring(p+1)].document; n=n.substring(0,p);}
  if(!(x=d[n])&&d.all) x=d.all[n]; for (i=0;!x&&i<d.forms.length;i++) x=d.forms[i][n];
  for(i=0;!x&&d.layers&&i<d.layers.length;i++) x=MM_findObj(n,d.layers[i].document); return x;
}

function MM_swapImage() { //Dreamweaver v3.0
  var i,j=0,x,a=MM_swapImage.arguments; document.MM_sr=new Array; for(i=0;i<(a.length-2);i+=3)
   if ((x=MM_findObj(a[i]))!=null){document.MM_sr[j++]=x; if(!x.oSrc) x.oSrc=x.src; x.src=a[i+2];}
}

function EmersonSearch()
{	searchwin = window.open("http://www.gotoemerson.com/search/sfrm.html","searchwin","width=325,height=100,scrollbars=no,toolbar=no");}

function GoUrl(s) {   
          if (s.options[s.selectedIndex].value == "here") {
             window.top.location.href = "http://www.frco.com/fr/";           
          } else {
		  window
          var d = s.options[s.selectedIndex].value
          //window.open(d)
		  window.top.location.href = d
          s.selectedIndex=0
        }
}

function MM_displayStatusMsg(msgStr) { // Dreamweaver v1.0
  status=msgStr;
  document.MM_returnValue = true;
}

function MM_goToURL() { // Dreamweaver v3.0
  var i, args=MM_goToURL.arguments; document.MM_returnValue = false;
  for (i=0; i<(args.length-1); i+=2) eval(args[i]+".location='"+args[i+1]+"'");
}